Sync Status - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.2

Metasys Performance Verification Tool (PVT) User Guide

Product
Accessories > Tools > Performance Verification Tool
Document number
LIT-12012406
Version
4.2
Revision date
2023-04-24

You can enable or disable sync status in Automatic scan mode or Interactive mode. The Sync status is set to Yes by default. If you select No, scans are not synced to the cloud.

Figure 1. PVT settings

Click Open Scan > Sync Status

The following table shows a series of conditions that would prevent a scan from syncing or not:
Table 1. Sync conditions
Settings Sync Status Work Hours Project Sync Status Will the project Sync?
Disable * * No
Enable Yes * No
Enable * External file No
Enable No Not external file Yes
Note: An external file refers to any scan that is not perfomed on the PVT application.
Note: This option is hidden by default. In order to display this option, set the value of HideSyncSetting=False in the JCI.Applications.PVT.exe.config file located in C:\Program Files (x86)\Johnson Controls\Metasys Performance Verification Tool.