Generating reports - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.2

Metasys Performance Verification Tool (PVT) User Guide

Brand
Metasys
Product name
Performance Verification Tool
Document type
User Guide
Document number
LIT-12012406
Version
4.2
Revision date
2023-04-24
Language
English

About this task

When you open a scan, you can generate a report that contains the scan data in a document format. You can export the report as a PDF or Microsoft Word document from the PVT Client, or PDF report only from the PVT cloud dashboard.

To generate and save a report of a scan, complete the following steps:

Procedure

  1. Open a scan. Click Open Scan in the toolbar or main menu, or click on the card of a recent scan in the main PVT window.
  2. Click Report in the upper right.
  3. Select the report type from the drop-down.

    The report window opens where you can scroll through the report.

  4. To change the page layout, click the Page Setup icon in the toolbar.
  5. To save the report, click the Export icon in the toolbar, and select PDF or Word.
  6. To print the report, click the Print icon in the toolbar.