Exporting scan results, a tasking estimate, and a tasking list - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.2

Metasys Performance Verification Tool (PVT) User Guide

Product
Accessories > Tools > Performance Verification Tool
Document number
LIT-12012406
Version
4.2
Revision date
2023-04-24

About this task

Note: These features are only available in the PVT client.

When you open a scan, you can export the scan results, a tasking estimate, or a tasking list into a Microsoft Excel file.

Note:

To export the scan data, perform the following steps:

Procedure

  1. Open a scan. Click Open Scan in the toolbar or main menu, or click on the card of a recent scan in the main PVT window.
  2. Click Export in the upper right and from the drop-down, select Scan Results, Tasking Estimate, or Tasking List.
  3. In the dialog window, change the file name if needed, and click Save.