The following table explains the different types of scans.
| Type of Scan | Description |
|---|---|
| Inventory | Identifies an inventory list of all controls hardware, such as supervisory devices and controllers, along with several key attributes of those controllers. |
| Performance | This feature performs the
following tasks:
|
| Feature Assessment | Measures how well the Metasys features are being utilized and reports on commonly underutilized features, such as Tailored Summaries, Optimal Start, or Demand Limiting/Load Rolling (DLLR). |