PVT hardware and software requirements - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.2

Metasys Performance Verification Tool (PVT) User Guide

Product
Accessories > Tools > Performance Verification Tool
Document number
LIT-12012406
Version
4.2
Revision date
2023-04-24
To install PVT successfully, we recommend the following hardware and software configurations:
  • Desktop operating systems:
    • Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). For all future Windows 10 updates after version 22H2, Johnson Controls will evaluate and certify that Metasys software can support the updates before we provide guidance on support.
  • Server operating systems:
    • Windows® 10 Pro - 2004,21H1,21H2 (64-bit)
    • Windows® Server® 2016 with Update (KB4512495) (64-bit)
    • Windows® 10 Pro and Windows 10 Enterprise Editions (version 21H2) (64-bit)
    • Windows® Server® 2019 (version 1809 or later) (64-bit)
    • Windows® Server® 2016 (version 1607 or later) (64-bit)
  • Connectivity
    • Broadband connectivity of 5 Mbps or greater to sync PVT scans to cloud without interruption (Autoscan mode)
  • Configuration:
    • <15 Engines: 8 GB RAM
    • 15-25 Engines: 16GB
    • 25 or more engines: 32GB
      Note: Ensure an additional 8GB of RAM is available to run PVT on a Metasys server machine.
    • 100 GB HDD
    • Microsoft .Net 4.7.2 or above
    • Microsoft Office® 2010 or above
    • Microsoft Visio® 2013 or above for exporting Riser view
    • SQLite® v3.27.2

Data Points in Autoscan mode

When PVT is installed on a Metasys server, the following server machine data points are captured by PVT:
  • Server Machine RAM usage
  • Server Machine CPU usage
  • USB port status
  • OS version
  • Hard drive free space
  • Firewall status
  • SQL version
Note:
  • If the Software Manager and SQLite v3.27.2 do not exist on the computer, the PVT installer automatically installs them during PVT installation. You do not need to remove any other SQL Server version that is installed on the computer.
  • If you install PVT on a server that runs ADS or ADX, the system requirements must match those outlined in Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin (LIT-1201525).
  • PVT UI works best with resolution settings 1920 x 1080. For the best viewing experience, set size of text, apps and other items to 100%.