Metasys Performance Verification Tool Cloud Dashboard - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.2

Metasys Performance Verification Tool (PVT) User Guide

Product
Accessories > Tools > Performance Verification Tool
Document number
LIT-12012406
Version
4.2
Revision date
2023-04-24
From PVT 4.2, you can use the Metasys PVT Cloud Dashboard to complete the following tasks:
  • Access Inventory data and Feature Assessment data reports. Refer to Inventory data, Feature Assessment data, and Performance data for more information about this data.
  • Generate customer facing pdf reports. You can generate Inventory data, Feature Assessment data, and Performance data reports.
  • Add and remove favorites from the Cloud Portal. You can now save sites as favorites to find scans associated with sites that you visit frequently.
  • Upload .pvt files to the cloud. Use this to manually upload a PVT file to the cloud repository in cases where a machine or site does not have access to the internet.
  • Download .pvt files from the cloud. You can download a .pvt file to a local machine and generate customer facing reports by opening the scan in the PVT client.
  • In autoscan mode, PVT supports backing up SCT archives (DBexport file only) to the cloud. This is only possible when SCT and PVT are installed on the same machine.
  • PVT can now measure MUI adoption, within a margin of error, for a given site. This includes the following metrics:
    • Count of spaces by type
    • Number of equipment objects
    • Number of points mapped to equipment objects
    • Equipment to space ratio
    • Ratio of controllers to equipment
    • Count of graphics by type
    • Metasys user login data
    The available metrics vary depending on which version of Metasys is installed at your site.
    Note: In order for PVT to pull MUI metrics from your site, you must use a Metasys user account that is assigned to the Access Type called API Access.
Figure 1. Metasys Performance Verification Tool Cloud Portal main menu