The following information is new or revised for PVT Release 4.2:
- Updated PVT hardware and software requirements.
- Custom installation is now supported. See Installing PVT for more information.
- In autoscan mode, you can now use the Site sync scheduler to change the schedule of a scan. See PVT user interface and Entering site configuration and scheduled scan data for information about this.
- PVT now supports scanning an OAS as server and engine, along with the objects, integrations and controllers within it.
- PVT in autoscan mode now supports retrieving scheduled backups of an SCT archive and syncing the dbexport to the cloud dashboard. Refer to Entering site configuration and scheduled scan data for more information.
- Added a new section Metasys Performance Verification Tool Cloud Dashboard.
- Updated Troubleshooting PVT to document an issue.