Feature Assessment data - Metasys - LIT-12012406 - Software application - Performance Verification Tool - 4.2

Metasys Performance Verification Tool (PVT) User Guide

Product
Accessories > Tools > Performance Verification Tool
Document number
LIT-12012406
Version
4.2
Revision date
2023-04-24

Feature Assessment searches for the use of the following Metasys features:

Table 1. Feature Assessment Tab
Feature Assessment Description
Metasys UI Location-based approach to finding information about the Metasys site.
Solar Clock Computes Present Value (Night or Day), Sun Position, and Sunrise/Sunset times based on local position and local time.
User Views User navigation view in Metasys.
Tailored Summaries Allows viewing and modification of large quantities of similar data in a tabular view in Metasys .
Optimal Start Aids in the reduction of energy costs during a building's transition from unoccupied to occupied. You can view and edit this feature in Metasys.
Demand Limiting/Load Rolling (DLLR) Helps save money by limiting energy use during times of peak demand. You can view and edit this feature in Metasys