Summary of Changes - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The following information is new or revised at Release 10.1:

  • Added content throughout for the new SNC and SNE network engines that are introduced at Release 10.1.
  • Added new attributes related to the release for devices, objects, and points.
  • Added two new objects supported by the ODS at Release 10.1: Channel Object and Lighting Output Object.