Annotating Objects/Items - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: In online mode with Basic Access, you cannot add an annotation to an object or item.

This feature allows you to enter follow-up comments for actions taken on this object or item, such as what the user did to fix a problem, what was fixed, or when an override was released.

To annotate objects/items:

Procedure

  1. Select the object/item to annotate in the navigation tree (All Items or User view).
    Note: You cannot add an annotation for a folder.
  2. On the Action menu, select Add Annotation.
  3. Select or type annotation text. Annotation text can be from 1 to 255 characters.
    Note: The Predefined Annotations List on the Add Annotation dialog box contains annotations saved in your system preferences. If you have not defined annotations in your system preferences, the drop-down list is empty.
  4. Click OK to save the annotation.