Configuring Annotation and Electronic Signature Requirements in the Site Object in MVE - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

For sites with MVE installed, configure the following attributes in the Site Object for MVE annotations and electronic signatures:

  • Annotation Include
  • Annotation Exclude
  • Annotation Alarm Priority Threshold
  • Signature Include
  • Signature Exclude
  • Signature Alarm Priority Threshold

These settings appear only on MVE sites. See the Site Object section for details on these attributes.

You can require annotations, electronic signatures, both, or neither on an MVE site. Non-MVE sites may optionally define and use annotations; however, electronic signatures are specific to MVE sites. For information on annotation and electronic signature preferences, see Annotation Settings Tab in the Preferences section. Also see Audit Message Annotations in Audit Trail for information on the fields in an annotation.

For additional information, refer to the Metasys for Validated Environments, Extended Architecture Technical Bulletin (LIT-12011327).