Temporary Override - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Temporary Override allows the operator to override a point for a specified time. After the specified time period passes, the Override is automatically released. At Release 8.1 and later, the Temporary Override command supports N2, LON, and VND integration objects.

Figure 1. Temporary Override Command Window

Note: The command duration can range from 1 minute to 100 hours, 59 minutes.
Table 1. Temporary Override Supported Objects
Local BACnet MSTP N2 LON VND
AV AO AO AO AO AO
BV BO BO BO BO BO
MSV AV AV MSO MSO  
  BV BV      
  MSO MSV     MSO
  MSV