Online Mode - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

When you are connected to the network engine or Metasys Server, you can perform online operational activities such as monitoring and commanding equipment. You can also perform online database configuration activities, such as defining field controllers or adding points. This function is referred to as online mode or online Site Management Portal (SMP) UI. The online mode is available to users with the Access Type of Standard Access or Basic Access. See the Access Types section.

Any changes you make to the system configuration are made online to the system and need to be uploaded to be stored in the archive database.