Offline Mode - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

SCT is a standalone software program installed on a computer that allows you to configure the servers and network engines without being connected to the live Metasys system server and network engines; this function is called the offline mode. In offline (system configuration) mode, use SCT to set up the system database. You must load configuration changes created in offline mode to the Engine for the settings to take effect. SCT can also be installed on the same computer as the ODS.

Two features are available only with SCT: ActionQ and Manage Archive. You can only add servers and network engines in offline mode.

The offline mode is available to users with the Access Type of Standard Access. See the Access Types section.