Warning Banner - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

After Metasys installation, you can use the SMP UI to enable a Warning Banner option at the Site object. The Warning Banner is a special login feature that consists of a text window that appears to the SMP user. The information in the text window is customized for the United States government agency where the Metasys system is installed. The user must read and accept the conditions set forth in the Warning Banner before logging in.

You have the choice of three different warning banners: U.S. Department of Defense (DoD), U.S. General Services Administration (GSA), or U.S. Department of Transportation (DOT) Federal Aviation Administration (FAA). The default selection is None. The following figure shows the Warning Banner selection in the UI.

Figure 1. Warning Banner Selection