Standard Access - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Standard Access allows the Metasys local system user, RADIUS, or Active Directory service user to access all authorized features of the online Site Management Portal (SMP) UI and the SCT.

Note: If you want to use the Metasys Advanced Reporting System, you must have Standard Access with the Advanced Reporting privilege.