Trend Viewer Table View - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Table view of the Trend Viewer allows you to view data for the selected trends in a table format. You can copy the trend data to the clipboard for pasting into other applications such as Microsoft Excel.

Note: The Historical Trend Icon appears in the Table View column headings when applicable.
Table 1. Table View

Button

Name

Description

Update

Updates the data samples with new trend data immediately.

Add

Allows you to add additional trend items to the Trend Viewer.

Copy to Clipboard

Allows you to copy selected trend data to the system clipboard for pasting into other applications such as Microsoft Excel. You can also use Ctrl + C to copy data to the clipboard.