Definition View Trend Items Table - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The Trend Items table appears at the bottom of the Definition view. The table displays the list of the Trend Viewer’s trend items.

Table 1. Definition View Trend Items Table

Button

Name

Description

Historical Trend Icon

Indicates the trend was selected from the ADSODS Historical Database folder.

Add

Opens the Select Item dialog box and allows you to add trend items to the Trend Viewer.

Remove

Allows you to remove a trend item from the Trend Viewer.

 

Name

Displays the name of the trend item.

 

Reference

Displays the trend item’s reference information.

 

Plotting Style

Allows you to select the plotting method for the trend item.

  • Continuous - straight line between data samples. Continuous plotting connects samples with the shortest possible line, giving an appearance of a set of diagonal ramps as samples change value.
  • Discrete - line stays at the same value until the next data sample is taken (good for binary data). Discrete plotting has 90-degree angles at the time when samples change value. The chart appears to be a series of steps.