Defining User Views with Summary Definitions - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Procedure

  1. Create a user view or edit an existing one (for example, an HVAC user view).
  2. Add a folder to the user view to hold the Summary Definitions. For example, add a Summary Definitions folder, or a folder named according to function (such as VAV Boxes - VMA1400s, Key Point Information, Engines, or MSTP Trunk Diagnostics).
  3. Drag the definitions from the Summary Definitions folder in the All Items tree to the folder you created in the user view (or use the user view editor’s add reference option).
  4. Drag the items to reference (for example, supervisory devices or points) from the All Items tree or from the global search results table to the folder in the user view (or use the user view editor’s add reference option).
  5. Save the user view.