Discarding Event Messages - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Procedure

  1. Launch the Event Viewer.
  2. Select one or more event messages.
    Note: Use the Ctrl or Shift key to select multiple messages.
  3. Click Discard.

    Notes:

    • Alternatively, you can right-click and select Discard or you can discard event messages in the Alarms Window. See Acknowledging, Snoozing, and Discarding Events for details.
    • In an Engine that is not the Site Director, acknowledged or discarded alarm and event messages do not appear acknowledged or discarded in the ODS.
    • An electronic signature or annotation may be required when discarding an event.