Configuring an Engine Event Repository - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

About this task

To configure the local Engine Event Repository and the Default Destination:

Procedure

  1. View an Engine device. See Viewing Item Data for information on how to display an item.
  2. Select the Focus tab and click the Advanced radio button to display additional item information.
  3. Select Edit.
  4. Scroll down to the Alarms and Site sections.
  5. Edit the attributes in these sections. Use the following table as a guide. See Engine Device Object for information about the attributes. The NAE Device attributes table contains Default Value and Values/Options/Range information for the attributes. Click the attribute names in the table for descriptions.
    Table 1. Repository Configuration

    To Do This:

    Edit This Engine Device Object Attribute:

    Change the size of the local Engine repository

    Alarm Repository Size

    Change the snooze time for the Alarms Window

    Alarm Snooze Time

    Forward acknowledged and discarded alarms and events from an NxE to the ODS repository

    Ack Forward Enable

    Designate an ODS repository as a Default Destination

    ODS Repository

    Indicate the type of connection used by the ODS

    ODS Connection Type

    Define a time to deliver event messages to the ODS

    ODS Delivery Time

    Define the event message priority that triggers delivery to the ODS

    ODS Priority Threshold

    Note: You can define only one repository as the Default Destination for an Engine. See Event Repositories for more information.
  6. Click Save.
    Note: If you want to define all local Engine repositories for the entire site at one time instead of individually, select the Site in the navigation tree and edit the following Site Object attributes (the Site attributes table contains Default Value and Values/Options/Range information for the attributes):
    • Default ADS Repository

    • Default ADS Connection Type

    • Default ADS Delivery Time

    • Default ADS Priority Threshold