Configuring Event Message Format - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Procedure

  1. View an Engine. See Viewing Item Data for information on how to display an item.
  2. Select the tab for the destination type.
  3. Select Edit.
  4. Select a destination in the Destinations section.
  5. Select the check boxes in the Format section to define which attribute information is included in the event message when delivered to that destination.
    Note: For example, select Value and Units if you only want to display the Value and Units portion of the event message at the destination.
  6. Click Save.