Configuring Encrypted Email with POP-Before-SMTP Authentication - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

About this task

Notes:

  • When SSL Email is enabled and you use POP-before-SMTP Authentication, the Metasys system uses port 995 to communicate to the mail server. Ensure that the mail server you are connecting to uses port 995 for secure socket layer connections for POP3 access.
  • When SSL Email is not enabled and you use POP-before-SMTP Authentication, the Metasys system uses port 110 to communicate to the mail server. Ensure that the mail server you are connecting to uses port 110 for non-encrypted POP3 access.

Procedure

  1. View an Engine. See Viewing Item Data for information on how to display an item.
  2. Click the Email tab.
  3. Click Edit.
  4. Edit the Attributes in the Shared Configuration as shown in Table 1.
    Table 1. Attributes for POP-Before-SMTP Authentication
    Attribute Selection
    SMTP Server Host mail.yourdomain.com or yourdomain.com
    SMTP Port 465
    Authentication Type POP-before-SMTP
    POP Server Hostname yourdomain.com or pop.yourdomain.com
    SSL Email Enabled True
    SSL Email Ignoring Errors False
  5. Verify that the email was sent successfully.