Configuring Encrypted Email with No Authentication Required - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: Encrypted Email with No Authentication Required functions only when Anonymous Authentication is enabled on the mail server.

Procedure

  1. View an Engine. See Viewing Item Data for information on how to display an item.
  2. Click the Email tab.
  3. Click Edit.
  4. Edit the Attributes in the Shared Configuration as shown in Table 1.
    Table 1. Attributes for No Authentication Required
    Attribute Selection
    SMTP Server Host mail.yourdomain.com or yourdomain.com
    SMTP Port 465
    Authentication Type None
    SSL Email Enabled True
    SSL Email Ignoring Errors False
  5. Verify that the email was sent correctly.