Applying Filters for Routing Event Messages to Destinations - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

Procedure

  1. View an Engine device object. See Viewing Item Data for information on how to display an item.
  2. Select the tab for the destination type (for example, Pager).
  3. Select Edit.
  4. Select a destination in the Destinations section.
  5. Select New in the Filters section. The Filter dialog box appears.
  6. Select a filter type from the Item drop-down menu. For more information and examples on filtering, see Event Message Routing, Filtering, and Destinations.
  7. Select the operator from the drop-down menu.
  8. Select a value from the drop-down menu or type the value in the text box.
  9. Click OK.
  10. Repeat step 4 through step 9 to add more filters to that destination.
    Note: If you define multiple filters for a destination, the DDA combines all the criteria with an AND condition (all filter criteria must be met).
  11. Make changes to filters using the drop-down menus or text boxes.
  12. To remove a filter, select a filter and click Delete.
  13. Click Save.