Adding Annotations - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

The annotation feature is not available on the local Engine event repository. You can add annotations to the ODS event repository only.

Procedure

  1. Launch the Event Viewer.
  2. Click the event message.
  3. Select Add Annotation from the Actions menu or right-click and select Add Annotation. The Add Annotation dialog box appears.
    Note: The drop-down field on the Add Annotation dialog box contains predefined annotations from your system preferences. If you have not defined annotations in your system preferences, the drop-down list is empty.
  4. Type the desired text in the message box.
  5. Click OK.