Filtering Options - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

You can apply filters to define which event messages are sent to specific destinations. For information on how to apply filters to event messages, see Applying Filters for Routing Event Messages to Destinations. Use the following table as a guide to defining filters.

Note: If you define multiple filters for a destination, the DDA combines all the criteria with an AND condition (all filter criteria must be met).
Table 1. Filters

Item

Operator

Value

Authorization Category

==, !=

HVAC, Fire, Security, Services, Administrative, General, Lighting, Refrigeration, Critical Environment, Air Quality, Power, Energy, System, or Custom Value

Acknowledge Required

==, !=

true, false

Current Status

==, !=

Normal, Fault, Off Normal, High Limit, Low Limit, Low Warning, High Warning, Low Alarm, High Alarm, Alarm, Trouble, Status, Offline, Shutdown, Unreliable, Online, Unknown Previous State

Previous Status (status prior to the event)

==, !=

Normal, Fault, Off Normal, High Limit, Low Limit, Low Warning, High Warning, Low Alarm, High Alarm, Alarm, Trouble, Status, Offline, Shutdown, Unreliable, Online, Unknown Previous State

Priority

==, !=, <, <=, >, >=

Range 0–255

See Event Priority.

Start Day of Week

==, !=, <, <=, >, >=

Monday through Sunday

Start Time

==, !=, <, <=, >, >=

The Time format is defined by the Language selected in the User Profile (User Profile tab of the Security Administrator System).

Example: HH:MM:SS AM/PM format (12:15:00 PM) for English Language selection

End Day of Week

==, !=, <, <=, >, >=

Monday through Sunday

End Time

==, !=, <, <=, >, >=

The Time format is defined by the Language selected in the User Profile (User Profile tab of the Security Administrator System).

Example: HH:MM:SS AM/PM format (12:15:00 PM) for English Language selection

For more information on filters, click the following section names: