Filtering Operators - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The following table describes the Boolean operators used to configure the filters for routing event messages to destinations.

Table 1. Operators

Operator

Meaning

==

Equal To

!=

Not Equal To

<

Less Than

<=

Less Than or Equal To

>

Greater Than

>=

Greater Than or Equal To

Note: If you define multiple filters for a destination, the DDA combines all the criteria with an AND condition (all filter criteria must be met).

For more information on filters, click one of the following section names: