Event Enrollment Configuration Example - Unsigned Range - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The following table is an example of how to configure an Event Enrollment Object using the Unsigned Range event type. In this example, the Event Enrollment object references the Present Value attribute of an Accumulator Object. An event message is generated as defined by its Event Enable attribute when the value of the Accumulator’s Present Value goes outside the user-defined low limit/high limit range for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.

Table 1. Unsigned Range Example

Tab

Attribute

Value

Focus

Event Enable

To Off Normal

Notify Type

Event

Event Message Texts Config

[1]: A potential excessive use fee

Input Reference

ACM1

Present Value

Delay Time (seconds)

120

Event

Low Limit

10000

High Limit

18000