The following table is an example of how to configure an Event Enrollment Object using the Out of Range event type. In this example, the Event Enrollment object references the Present Value attribute of an Analog Input Object. An event message is generated as defined by its Event Enable attribute when the value of the AI’s Present Value attribute goes outside the user-defined low limit/high limit range for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.
Tab |
Attribute |
Value |
---|---|---|
Focus |
Event Enable |
To Off Normal |
Notify Type |
Event |
|
Event Message Texts Config |
[1]: Room Temp Out of Range |
|
Input Reference |
AI1 Present Value |
|
Delay Time (seconds) |
300 |
|
Event |
Low Limit |
66.0 |
High Limit |
74.0 |
|
Deadband |
2.0 |