The following table is an example of how to configure an Event Enrollment Object using the Change of State event type. In this example, the Event Enrollment object references the Reliability attribute of a Multistate Value Object. An Event message is generated as defined by its Event Enable attribute when the state of the MV’s Reliability attribute changes to Unreliable for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.
|
Tab |
Attribute |
Value |
|---|---|---|
|
Focus |
Event Enable |
To Off Normal |
|
Notify Type |
Event |
|
|
Event Message Texts Config |
[1]: Point is now Unreliable |
|
|
Input Reference |
MV1 Reliability |
|
|
Delay Time (seconds) |
0 |
|
|
Event |
Event Type |
Change of state |
|
Value |
Unreliable |