The following table is an example of how to configure an Event Enrollment Object using the Change of Bitstring event type. In this example, the Event Enrollment object references Status flags of an Analog Value Object. An event message is generated as defined by its Event Enable attribute when either the In Alarm or Fault attribute changes to True for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.
|
Tab |
Attribute |
Value |
|---|---|---|
|
Focus |
Event Enable |
To Off Normal |
|
Notify Type |
Event |
|
|
Event Message Texts Config |
[1]: Change in Status Detected |
|
|
Input Reference |
AV1 Status Flags |
|
|
Delay Time (seconds) |
10 |
|
|
Event |
Mask |
In Alarm - selected (true) Fault - selected (true) Overridden - not selected (false) Out of Service - not selected (false) |
|
Values |
In Alarm - selected (true) Fault - selected (true) Overridden - not selected (false) Out of Service - not selected (false) |