Alarm and Event Management - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The alarm and event feature provides event management for the Metasys system. This feature allows you to configure the detection of alarm conditions and the routing of event messages to destinations such as an email account or pager for acknowledgment. The Alarms Window displays event messages in a prioritized order and allows you to respond to the alarms. The Event Viewer provides the functionality to retrieve and examine event messages stored in an event repository.

For information on alarm and event management for Metasys systems integrated with BACnet devices, see the Alarm and Event Management for Metasys Systems Integrated with BACnet Devices topics.