Enabling Advanced Auditing - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

At Metasys UI Release 2.0 and later, the Equipment Activity widget captures audits of commands performed by Schedule objects, Multiple Command objects, and Interlock objects that are tied to equipment configured to the Metasys UI. To utilize this feature, the Engine object must be at Metasys Release 8.0 or later and the Enable Application Generated Audits attribute must be set to True.

Procedure

  1. In , open the Engine object's tab.
  2. Select Advanced.
  3. Click Edit.
  4. Under the Audit Trail section, change the Enable Application Generated Audits value to True.
  5. Click Save .