Configuring the Engine Audit Repository - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

About this task

To configure the Engine Audit Repository and the Default Destination:

Procedure

  1. View the Engine device. See Displaying Information About an Item for information on how to display an item.
  2. Select the Focus tab, and click the Advanced radio button to display additional item information.
  3. Select Edit.
  4. Scroll down to the Audit Trail and Site sections.
  5. Edit the attributes in these sections. Use the table below as a guide. See the Engine Device Object chapter for information about the attributes. The Engine Device attributes table contains Default Value and Values/Options/Range information for the attributes. Click the attribute names in the table for descriptions.
    Table 1. Configuring the Engine Audit Repository

    To Do This:

    Edit This Engine Attribute:

    Change the size of the Engine local audit repository.

    Audit Repository Size

    Designate an ODS repository as a Default Destination.

    ADS Repository

    Define a time to deliver audit messages to the ODS.

    ADS Delivery Time

    Define how full the audit repository must be before forwarding audit messages to the ODS.

    Dial-Up Audit Forwarding Threshold

    Define if the Audit Trail feature overwrites existing audit messages or stops generating audit messages when the audit repository is full.

    Note: This action is only valid when the device is not set to forward data to an ODS. The stop/rollover option only applies when there is no forwarding to an external repository.

    Audit Action When Full

    Define if the Audit Trail feature should generate an alarm when the audit repository is full.

    Audit Generate Alarm When Full

    Define which level of audit messages get added to the audit repository.

    Enabled Audit Level

    Note: You can define only one repository as the Default Destination for audit messages from an Engine audit repository. See Audit Repositories for more information.
  6. Click Save.
    Note: If you want to define all Engine local repositories for the entire site instead of individually, select the Site in the navigation tree and edit the following Site Object attributes. The Site object attributes table contains Default Value and Values/Options/Range information for the following attributes:
    • Default ADS Repository
    • Default ADS Delivery Time