Adding Annotations - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: You can add annotations from the ODS only. Annotations are not forwarded between ODSs.

Procedure

  1. Launch the Audit Viewer by selecting the ODS from the Device Selection Dialog box.
  2. Right-click the audit message, and select Add Annotation from the menu. Alternatively, you can select Add Annotation from the Actions menu. The Add Annotation dialog box appears.
    Note: The drop-down list on the Add Annotation dialog box contains predefined annotations from your system preferences. If you have not defined annotations in your system preferences, the drop-down list is empty. .
  3. Type the desired text in the message box.
  4. Click OK.