Audit Trail - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Audit Trail feature generates audit messages and stores them in Audit Repositories. An audit message contains information about a significant event on the BAS. For audit purposes, a significant event is an action or occurrence on the system that should be recorded for later analysis of building operations. A new audit message is generated for each significant event on the BAS. The Audit Message and Audit Viewer displays the audit messages stored in an audit repository. You can access the Audit Viewer from the View Menu of the Metasys user interface in online mode.

The Audit Trail provides a historical record of the audited events, such as creating or deleting items, that have occurred within the system. By viewing audit messages, you can examine and analyze the actions that occurred in the system.