Menu Selection: (select the check box)
Toggles the display of the item labels in the All Items navigation tree or user navigation tree from standard to extended. An extended label shows the BACnet object name that was defined when the object was initially created in braces next to the standard label. This is the name used in the object's Fully Qualified Reference. The Metasys object name may be the same as the BACnet object name, or it may have been edited as a label that is more recognizable to the user.
Example:
Standard Label = N2 Trunk1
Extended Label = N2 Trunk1{N2-1}