Enable Alarm Pop-Ups - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

Menu Selection: View > Enable Alarm Pop-Ups (select the check box to enable/disable alarm pop-ups)

For the current user session, this item determines if the pop-up Alarms Window (also referred to as Metasys - Events or Alarm Bar) automatically displays when an alarm is detected.

Clicking the alarm icon in the status bar re-enables alarm pop-ups and displays the current alarm, if any.

If you disable the alarm pop-up window and you have the audible alarm option enabled, the audible alarm sounds when an alarm is detected. See the Alarms Window section in the Site Management Portal User Interface.