The Change Results Viewer displays the result entries for the global commands and global modifications sent during the current user session. You can access the Change Results Viewer by selecting Change Results from the View Menu.
Column/Button |
Description |
---|---|
Change Results Table |
Displays the results of all global commands/modifications sent during the current user session. If you select an item in the table and place your cursor over it within each column, tooltips appear providing more information, if available. Any data that does not fit within the columns is identified by an ellipsis (. . .). You can resize the column or place your cursor over the table cell to see its tooltip text. If you send another global command/modification at a later time during the current user session, the result entries are added to any existing result entries from prior commands/modifications sent during the session. The most recent entry appears at the top of this table by default. If desired, you can sort the results. See the Working with the Change Results Viewer section for more information on manipulating and using the table data. |
When |
Displays the date and time the command/modification was sent. |
Item |
Displays the name of the object to which the command/modification was sent. The object’s full reference identifier appears in a tooltip when you place the cursor over the name. |
Change Type |
Displays the type of command/modification sent. |
Parameters |
Displays the list of parameters for the command/modification that was sent. For example, for a Release command, an attribute and priority such as Present Value, 15 (Scheduling) appear in the Parameters column. |
Status |
Displays the status of the command/modification that was sent (for example, OK or an explanation of failure). Notes:
|
Clear Results Viewer |
Deletes all the entries from the Change Results Viewer and adds an entry to indicate when it cleared those entries. |
Copy |
Copies the selected change results to the Clipboard for pasting into other applications such as Microsoft Excel® or Word®. |
Save to File |
Saves the current content of the change results table to a text file. |