System Preferences - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

System preferences apply to all users who log in to the site or device. System preferences affect the performance and operation of the system and require authorization to configure. A change to the audible alarm notification is an example of a system preference. Only the users defined in the Users Authorized to Edit System Preferences section are authorized to configure system preferences.

To synchronize system preferences within a site or to reuse the system preferences on another site, refer to the Configuring and Maintaining Preferences appendix of the ODS Commissioning Guide (LIT-12011944) or the NAE Commissioning Guide (LIT-1201519).