The Annotations Settings tab allows you to define customized annotations to select when acknowledging and discarding events.
You can configure annotations at the device and object levels. Also see Configuring Annotation and Electronic Signature Requirements in the Site Object in MVE.
Table 1 describes the attributes of the Annotation Settings tab.
|
Field Name |
Description |
|---|---|
|
Annotation Text |
Enter a new annotation to be added to the list of predefined annotations. The text can be from 1 to 255 characters in length. Click Add to save the new annotation. Predefined annotations can be edited or deleted. |
|
Predefined Annotation List |
Displays the list of predefined annotations. Select a reason and click Delete to remove the annotation from the list. The Move Up and Move Down buttons allow you to reorder the list. |