Metasys Preferences Dialog Box - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Metasys Preferences dialog box is accessed through the Tools menu (Configure Preferences) and allows you to configure system and user preferences. Users authorized to edit system preferences can edit all preference fields using the Metasys Preferences dialog box. See Users Authorized to Edit System Preferences. Unauthorized users can edit only user preferences.

Some of the preferences defined in the Metasys Preferences dialog box also apply to the Metasys UI. The following table calls out the tabs with such preferences. See the specific tab section for details.

Click the tab name in the table for a description of the Metasys Preferences tabs. For more information on the modes of operation, see Metasys Modes. The Authorization Required column means you must be authorized to edit some or all of the preferences located on that tab.