User Defined States Text - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Prior to Release 6.0, States Text was auto generated for third-party BACnet® Objects devices during the online discovery process within the Metasys system. Once the states text was discovered online, the information could be uploaded into an SCT archive for storage.

At Release 6.0 and later, User Defined States Text sets can be created both online or offline in SCT. The new Custom Enumeration tab has been added to the Site Object, which allows the creation of new enum sets that can be applied to any Binary or Multi-Value Objects.

Note: If you create a custom enumeration set that has only two members, the set does not appear in the list of sets for a Multistate Value Object.