HVAC PRO Name Restrictions in Passthru Mode - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

HVAC PRO Release 8.06 and later restricts the number of characters allowed in each controller name. HVAC PRO does not download, upload, commission, or retrieve information about the controller if the item name or controller name exceeds the 157 maximum characters limit.

The controller’s full name consists of the following: domain name, site name, equipment name, trunk name, and the actual controller’s name. The controller name appears in the following format:

Site_name:device_name.domain_name/N2 Trunk #.controller_name

The following table describes the controller name restrictions.
Note: The component column lists each of the components represented in a Full Item reference. The Maximum Viewable Characters column lists the restrictions on the Component names when entered through SCT or a web-based user interface of the Metasys supervisory controller. The Maximum Characters Allowed by HVAC PRO column shows the maximum number of characters in a Full Item Reference allowed in HVAC PRO.
Table 1. Controller Name Restrictions

Component

Maximum Number of Characters Allowed by the Engine or SCT

Maximum Viewable Characters

Maximum Characters Allowed by HVAC PRO

Site Name

fewer than or equal to 32

30

47 Total

157

Device Name

fewer than or equal to 15

Domain Name

fewer than or equal to 64

N2 Trunk Name

fewer than or equal to 32

-

Controller Name

fewer than or equal to 32