Administrator - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Menu Selection: Tools > Administrator

Launches the Security Administrator System. This menu item is only available for users in the ADMINISTRATOR role. Within the Security Administrator System, Administrators manage user accounts by creating roles/profiles; setting user passwords; assigning category-based, system-level, and navigation view permissions/access; and performing other duties. The same set of administrative management is available in Metasys UI Online, which is now preferred over the Security Administrator System in SMP.

For more information on the Security Administrator System in SMP, refer to the Security Administrator System Technical Bulletin (LIT-1201528). For more information on the Security Administrator System in Metasys UI Online, refer to the Settings, Security, and Authorization for Metasys UI section in Metasys UI Help (LIT-12011953).