Creating a Repeating Yearly Report - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To create a repeating yearly report that runs on the last day of February:

Procedure

  1. Repeat step 1 to step 4 in Creating a Daily Report.
  2. Select Run This Report Yearly.
  3. Enter the Start Date.
  4. Enter the End Date.
  5. In the Date Information section, select Feb and Last from the drop-down menus.
  6. In the Time Information section, configure the Run At time information.
  7. Click Save.
    Note: If it is a leap year, this report runs on February 29th; otherwise, it runs on February 28th.