Creating a Repeating Weekday Report - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To create a new report that runs every hour on weekdays between the hours of 11:00 A.M. and 1:00 P.M. with an end date of two months from today:

Procedure

  1. Repeat step 1 to step 4 in Creating a Daily Report.
  2. Select Run This Report Weekly.
  3. Verify the Start Date is set to today.
  4. Configure the End Date to two months from today.
  5. In the Date Information section, select the Mon - Fri check box.
  6. In the Time Information section, configure the Run At time to 11:00 A.M.
  7. Select the Repeat check box. The Until and Every fields enable.
  8. Configure the Every field to 60 minutes.
  9. Configure the Until field to 1:00 P.M.
  10. Click Save.