Creating a Repeating Monthly Report - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To create a repeating monthly report that runs on the 15th and last day of every month at 8:00 A.M. with no end date:

Procedure

  1. Repeat step 1 to step 4 in Creating a Daily Report.
  2. Select Run This Report Monthly.
  3. Verify the Start Date is set to today.
  4. Select the No End Date check box.
  5. In the Date Information section, select 15 and Last (Ctrl + click).
  6. In the Time Information section, configure the Run At time information to 8:00 A.M.
  7. Click Save.