Creating a Daily Report - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

About this task

To create a new report that runs every day at 8:00 A.M. with no end dates:

Procedure

  1. On the Query menu, select New Scheduled Report. The Create New Scheduled Report Dialog Box appears.
  2. Enter a report name that has fewer than 100 characters.
  3. Select an Object List to run the report against.
  4. Select a Report Format.
  5. Select Schedule Report.
  6. Select Run This Report Daily.
  7. Verify the Start Date is set to today.
  8. Select the No End Date check box.
  9. In the Time Information section, configure the Run At time to 8:00 A.M.
    Note: Do not configure Repeating Information.
  10. Click Save.